How do you use the Reference field on the Scale command?

2021-10-06T23:53:56Z

Summary


Details

How do you use the Reference field on the Scale command?



Solution

For the case where you have an existing length and you have a length that you wish to scale that existing length up to, you can use the Reference field as follows. Set the Reference field to the existing length. Click one end of the length as the origin for the scale. Drag the other end of the existing length to the desired value. This works well if you have two lines with a common origin: the existing line and another line that is drawn to the desired length.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V219MP4
Function: GEOMETRY

Ref: 001-9382413

KB Article ID# PL8008183

Contents

SummaryDetails

Associated Components