Details
Warning message "This drawing refers to an assembly that is not up to date. Open the assembly and check it out, then check out all candidate assemblies, synchronize the structure, then save the synchronized structure to Teamcenter" displayed when open the draft that the released assembly projected.
Solution
This message appears when open draft is because it found the linked assembly has structure modified (based on BOM's Modified time which get changed when the structure become precise).
Additionally, if you open the particular assembly separately then also we will get the BOM Sync message. This is because as per our current architecture if the BOM modified time is later than file uploaded time then we show BOM sync message. This behavior is currently as per design.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC
Ref: 002-8008171