How to control the precision of the hole size in the Hole Table.

2021-10-06T23:53:53Z

Summary


Details

Example on how to change the hole size to 4 decimal places in the Hole Table.



Solution

Here is an example on how to change the hole size to 4 decimal places in the Hole Table:

Right Mouse Button on the Hole Table and select 'Properties'. Go to the Column tab. Click on 'Columns -> Size'. Modify the 'Property text, so that it reads "%{%HS/@4}" (no quotes) and click on 'Apply'. The formatting syntax can be found in Help, under the topic 'Format codes to modify property text output'.

The link below has details for 'Property text codes'.


http://docs.plm.automation.siemens.com/tdoc/se/2019/se_help/#uid:symtxt1d



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V219.0
Function: TABLES

Ref: 001-9366216

KB Article ID# PL8007985

Contents

SummaryDetails

Associated Components