How to map Arialn Autocad font to Solid Edge ANSI font?

2021-10-06T23:53:52Z

Summary


Details

How to map arialn Autocad font to Solid Edge ANSI font.



Solution

Click on 'Application button -> Save As -> Save as Translated'. Set 'Save as type' to dwg or dxf. Click on the 'Options' button and then click on 'Next' until you get to 'Solid Edge to AutoCAD Translation Wizard - Step 5 of 7'.  Locate 'seans.ttf,  which is the default mapping to Solid Edge ANSI. Here it gets a little tricky to override the Autocad font;  you have to click on 'seans.ttf', wait a second and then click again (not a double click). Type 'Arialn.ttf'. This sets the mapping to Solid Edge ANSI. Click on 'Next' until you get to the dialog to 'Create a new configuration file' and click on 'Finish'.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219.0
Function: AUTOCAD

Ref: 001-9365497

KB Article ID# PL8007971

Contents

SummaryDetails

Associated Components