Why is a PAX file using this entry - <ObjectData class="AeroSheetMetalTemplate"> - failing with the following error in the log file?
"No TemplateValidator found for template aero-sheet-metal-inch-template.prt, application type AeroSheetMetalTemplate. Template ignored."
Solution
This entry - <ObjectData class="AeroSheetMetalTemplate"> - in the PAX file means the user wants to use that template to launch "Aerospace Sheet Metal" application. Per NX documentation below, Aerospace Sheet Metal has been retired, so it is not valid to pass the Template validator.
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#uid:index_whatsnew:id1241822:xid1098565:xid1098557
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 2008_R2
Product: NX
Application: ASSEMBLIES
Version: V11.0.2
Function: PART_FILE_OPS
Ref: 001-9362297