How to automatically create gaps in dimension extension lines

2021-10-06T23:26:35Z

Summary


Details

How to automatically create gaps in dimension extension lines when text values from other dimensions cross over it.



Solution

When creating or editing the dimension:
1. On the Linear Dimension dialog (under the Settings grouping), select the 'Settings' icon.
2. Browse to 'Line/Arrow-->Break'.
3. Toggle ON "Create Breaks". 

This is also a Drafting Preference.
1. In the Menu, select 'Preferences-->Drafting'.
2. 'Common-->Line/Arrow-->Break'.
3. Turn ON/OFF "Create Breaks".



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DIMENSION

Ref: 001-9361300

KB Article ID# PL8007953

Contents

SummaryDetails

Associated Components