Is it possible to create a line by center as we can do with a rectangle or a circle by center?
Solution
Select the command line, then click on the point you want to be the center, then press "S" and now you are placing the line with the endpoints symmetric about your first point.

Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V219.0
Function: DYNAMIC_EDIT
Ref: 002-8007910