How to disable the CADENAS Library

2021-10-06T23:26:34Z

Summary


Details

How to disable to CADENAS Library for all users



Solution

The only way to currently hide this library is to remove it from all applications.

Before beginning, back up this file:  C:\Users\<<userid>>\AppData\Local\Siemens\NX120\ReuseLibraryConfiguration.krx

1. Exit NX.
2. Open this file in a text editor.
   C:\Users\<<userid>>\AppData\Local\Siemens\NX120\ReuseLibraryConfiguration.krx
3. To remove the applications it is available in, simply delete the "Application" lines for this CADENAS Library, and re-save the file.
4. Have all users exit NX.
5. Move the modified ReuseLibraryConfiguration.krx file to UGII_SITE_DIR\startup
6. In Customer Defaults (Gateway-->Reuse Library-->General (tab)), set the Shared Library Configuration File to "Native File System" and point to the modified file: 
    UGII_SITE_DIR\startup\ReuseLibraryConfiguration.krx

Please NOTE: There is a big disadvantage to this...the user's ReuseLibraryConfiguration.krx will take precedence over this global file, so you will need to make sure to remove the ReuseLibraryConfiguration.krx from all user's NX folder (C:\Users\<<userid>>\AppData\Local\Siemens\NX120\) while they are out of NX.



Notes and References

ER #8405435 - Need customer default to remove Cadenas Reuse Library for all users easily

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V12.0.2
Function: REUSE_LIBRARY

Ref: 001-9356293

KB Article ID# PL8007865

Contents

SummaryDetails

Associated Components