I have some trouble activating the new NX1847 version.When I start NX I get the info that the server_id function isn't compatible with the version of the application.
I've installed the actual version of the PLM license server (version 9.1) which comes with the download of the NX 1847 files.
Please perform these tests in this numbered sequence :
1)Please delete your splm_ugslmd.log before restarting your License Server.
2) Please, instead of using "Reread" functionality on Flexlm License Server ... ... use : 2a) Simple procedure : please reboot your PC after having changed the license file inside the SPLM License Server directory. 2b) or you can use a more complex procedure, for more expert System Users : - STOP Siemens PLM License Server service - change the license file and replace the old one with the correct one - START the same service