A change to the Easy Fill application NX12 v3 requires that the NX Pre/Post application be installed.
The EasyFillAdvancedNX12_data_v3_README states:
Requirement:
------------------------
Please check whether "simulation pre/post application" has been installed.
Solution
The NX CAE mesh API will be called in Easy Fill NX12 v3, so users should make sure "simulation pre/post application" has been installed. Users can check whether they have this application installed as following picture. Please note: user should have this application installed, but they needn't have this license.

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V12.0
Function: MOLDWIZARD
Ref: 002-8007763