Solid Edge Request help with TeamCenter data Set Sequence . . .

2021-10-06T23:53:48Z
Design

Summary


Details

How do you retrieve a sequence from a Solid Edge dataset using Teamcenter (RAC) without having it open read only in Solid Edge?  Need to replace the current dataset with a previous sequence.



Solution

The approach is to use RAC to download the file you want (from the sequence). Then while in the RAC go to the current ItemRev containing the same file and via name reference delete the current file and upload the older file ( from the sequence). Please note we are not able to guarantee this method will be a valid substitution in the CAD world once you open any assemblies or other files that have a relationship to the substituted file. This is why we don't allow this via SEEC..... we have no idea what file relationships may break when working outside the CAD tool.. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: DATA_PREP

Ref: 001-9344097

KB Article ID# PL8007753

Contents

SummaryDetails

Associated Components

Part Modeling