Simcenter 3D Solutions Solution Monitor hangs with Nastran solve

2021-10-06T23:26:34Z
Simcenter 3D

Summary


Details

When launching a NX Nastran solution the solution monitor starts, and then hangs and never updates again. Works in previous versions of NX but fails in 2019.1.

Solution

Found that the customer had an old UGII_TMG_DIR variable defined. This variable is used to point to a different version of the Thermal and Flow solver. The solution monitor is shared between the Thermal and Flow solver and NX Nastran. In this case, the UGII_TMG_DIR variable pointed to a previous version of the Thermal and Flow solver that was not working correctly with 2019.1. Deleting the UGII_TMG_DIR variable resolved the issue.

Notes

KB Article ID# PL8007736

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow