Details
How can I suppress assembly relation from excel file.
Solution
You can use the Suppression Variable command to add a suppression variable to the variable table. A value of 1 (one) indicates that the relationship is suppressed. A value of 0 (zero) indicates the relationship is unsuppressed. Formulas in the variable table can be used to suppress assembly relationships when the value of the variable meets the criteria defined by the formula. This suppression variable from variable table can be linked with excel data cell by using paste ling and then can be controlled by changing value from excel.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219MP3
Function: RELATIONS
Ref: 002-8007716