When double clicking the Application button, Solid Edge will close. Is this as designed or is it a bug?
Solution
This is a Microsoft feature - the Application button in Microsoft Office does the same:
https://www.howtogeek.com/howto/20797/stupid-geek-tricks-double-click-the-left-window-icon-to-close-an-app-in-windows/
So this is working as designed.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: APPLICATION
Version: V219MP4
Function: UI
Ref: 001-9348323