When opening a model from Teamcenter into Teamcenter Visualization, the name of the model being opened is "MODEL", not the actual name of the model (ie - 000027).
Here is an example.

Solution
This is due to the model not being saved from NX while the environment variable UGII_GENERATE_MULTI_CAD_JT=1 is NOT set. Setting this variable at the OS will result in a properly named part file.
Here is an example:

Hardware/Software Configuration
Platform: AMD64
OS: window
OS Version: 1064
Product: NX
Application: TRANSLATOR
Function: NX_JT
Product: TC_VISUALIZATN
Application: VISVIEW
Function: ASSEMBLY_TREE
Ref: 002-8007699