Solid Edge Unable to configure Solid Edge with the Inventor Data Migration tool.

2021-10-06T23:53:45Z
Apps

Summary


Details

When configuring the Inventor Data Migration tool, not able to select a root folder and subfolder where the Inventor files are located. 

 

Solution

The Inventor Data Migration command assumes that Inventor is installed on a computer somewhere on your network. Solid Edge supports only Inventor version 6 or later.


If you are running Inventor version 9 or greater, use the DXF/DWG export utility to disable the Pack and Go parameter.






Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS

Ref: 001-9344124

KB Article ID# PL8007676

Contents

SummaryDetails

Associated Components

Translators