Solid Edge What is the Rip Corner command in sheetmetal used for?

2021-10-06T23:53:43Z
PART/SHEETMETAL

Summary


Details

What is the Rip Corner command in sheetmetal used for?

Solution

The Rip corner command rips the edge of a model or curve, producing two new faces. This creates a gap in the model. Separating the faces is necessary to convert many imported models and models created with part features, such as a thin-walled protrusion.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219.0
Function: FEATURES

Ref: 002-8007660

KB Article ID# PL8007660

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN