Solid Edge What is an intent zone?

2021-10-06T23:53:42Z
Design

Summary


Details

What is an intent zone?

Solution

Solid Edge uses intent zones to interpret your intentions as you draw and modify elements. Intent zones allow you to draw and modify elements many ways using few commands. You do not need to select a different command for every type of element.

For example, when you draw an arc by three points, the third point can be either an end point of the arc or a point along the arc (between the end points). You can also change the convexity and direction of the arc as you input the third point. These options are available simply by moving the cursor through an intent zone.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V219.0
Function: OTHER

Ref: 002-8007658

KB Article ID# PL8007658

Contents

SummaryDetails

Associated Components

Part Modeling