NX X Showing part display changes in the assembly

2021-10-06T23:26:33Z
NX for Design

Summary


Details

Changes made during an 'Edit-->Object Display' operation on a part are not showing up in the assembly‰. Why?



Solution

1. In the Assembly Navigator, highlight the component that is not showing the Object Display changes.
2. 'MB3-->Properties'.
3. Select the 'Assembly' tab.
4. Is "Specific Component Color" turned ON? If so, turn this OFF.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V10.0.3
Function: ASSEMBLY_MODEL

Ref: 001-9342885

KB Article ID# PL8007601

Contents

SummaryDetails

Associated Components

Assemblies