Solid Edge Transfer button is greyed out in an assembly having FOA (Family of Assembly) member.

2021-10-06T23:53:39Z
Design

Summary


Details

Transfer button is greyed out in an assembly having FOA member. 

Solution

For alternate assembly the Transfer command is only available when the 'Apply Edits to All Members' option is set. If this option is unchecked then 'Transfer' button is greyed out. 


This option is available on Alternate Assembly Pane. When you set the Apply Edits to All Members option on the Alternate Assemblies tab, the modifications you make are globally applied to all members.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V110MP7
Function: FOA/AP

Ref: 002-8007580

KB Article ID# PL8007580

Contents

SummaryDetails

Associated Components

Assembly Modeling