Solid Edge SEEC : Which Solid Edge release is compatible with TC 12.1.0.0 and AW 4.1?

2021-10-06T23:53:38Z
DOC_MANAGEMENT

Summary


Details

Which Solid Edge release is compatible with Teamcenter 12.1.0.0 and Active Workspace 4.1?



Solution

As of 31-DEC-2018: Solid Edge 2019 Maintenance Pack 1 (2019 MP1) is certified to be compatible with Teamcenter 12.0 and Active Workspace 4.0. The SEEC Feature package for Teamcenter 12 is included in the SEECAdmistratorV219.zip for MP01. Teamcenter 12.0 includes the new functionality introduced in Teamcenter 11.5, enabling a Teamcenter rich client user to configure a product structure and open it in Solid Edge. 

Solid Edge 2020 is currently in a certification cycle with TC12.1 & AW 4.1. SE 2019 MP will also be certified. Release dates projected for early first quarter 2019. 

Solid Edge End of Maintenance: End of Maintenance dates for the Solid Edge suite of products are listed in SFB-SOLID_EDGE-8000986 

<https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=SFB-SOLID_EDGE-8000986&file_type=html&i=sfb-solid_edge-8000986&k=0&o=0>. 

These dates represent when Siemens PLM Software will discontinue development activities and Maintenance Pack delivery along with the last Teamcenter release supported. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP7
Function: SEEC

Ref: 001-9336088

KB Article ID# PL8007563

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC