NX X Move a pole to an existing point using X-Form

2021-10-06T23:26:33Z
NX for Design

Summary


Details

In Pre-NX8, the Move Pole function had an option for "Move to a Point" that can be used to select an existing point to move a pole. In X-form, how can a pole be moved to an existing point? 



Solution

In X-Form, before selecting the pole turn on the Snap-Point option that needs to be used, (i.e Existing Point), then pick and drag the pole to the existing point and release it. The pole will now be associated to the point. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: STUDIO_DESIGN
Version: V11.0
Function: FREE_FORM

Ref: 001-9335539

KB Article ID# PL8007520

Contents

SummaryDetails

Associated Components

Modeling