How to enable Process Simulate 3D PDF option for generating 3D PDF

2021-10-07T00:01:27Z

Summary


Details

While generating 3D PDF dataset from Process Simulate on Teamcenter "Process Simulate" option is greyed out.



Solution

For enabling "Process Simulate" option for generating 3D PDF dataset use the below steps
 1) In Teamcenter (MPP Application), Select the  Process Revision and right click ->select Open with process Simulate to load the Process Revision and operations in PS.
 2) Right click on Menu bar ->Select option "Customize the Ribbon" option from available option.
 3) In Customize window add "Create 3D Documentation" from Choose commands from to Customize the Ribbon ->Click on Ok.
 4) Once you add "Create 3D Documentation" option in New tab in Process Simulate -> Select Process from Object Tree window in PS and Click on Create 3D documentation->Select the "view" for operations  in steps to create  table >Click on Generate tab to generate 3D PDF.
 5) Then Click on Teamcenter Update in Process Simulate to update the PDF in Teamcenter from Process simulate.
 6)Go to Teamcenter, Select the Process Revision -> Go to Tools ->Generate 3D PDF Report ->Select "Create a new report" in Generate PDF Report Wizard window -> Enter the name and click on Next ->Select  3D PDF template from templates option ->Process Simulate option Should be enable for generating the 3D PDF.



Notes and References

Use the below link for documentation.
https://docs.plm.automation.siemens.com/tdoc/tecnomatix/14.1/PS_TC#uid:index_xid1015772:xid1132064:xid1169102:id1246454186982

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: XP64_SP1
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.1.1
Function: BACKBONE_INTEG

Ref: 002-8007487

KB Article ID# PL8007487

Contents

SummaryDetails

Associated Components