Siemens PLM Licensing Hardware and Software Requirements for 3 Redundant servers

2021-10-06T23:26:33Z
Licensing Maintenance

Summary


Details

Hardware and Software requirements for Three Redundant Server license




Solution

Siemens PLM Licensing does not provide specific requirements and do not officially certify them (alike it is done with graphic cards). One of reasons is that we simply cannot predict what customer installation will be in term of load and license server configuration (multiple servers, redundant servers and so on). The main reason is that the underlying technology (FlexNet Publisher, aka FlexLM) does not provide such information as well.


 


In general, licensing is not demanding to resources at all, one does not need powerful servers to run. The networking configuration is more important as well as general license server topology (multiple/redundant servers, where they are located, latencies and so on)



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSTEM
Version: V12.0
Function: SYSTEM_TOOLS

Ref: 002-8007478

KB Article ID# PL8007478

Contents

SummaryDetails

Associated Components

Siemens PLM Common Licensing