Tecnomatix Is Process Simulate installation supported on the Virtual Infrastructure (VDI)

2021-10-07T00:01:27Z
Process Simulate

Summary


Details

Is Process Simulate installation supported on the Virtual Infrastructure (VDI)

Solution

The Tecnomatix 14.0 setup has a documentation process which contains the "TecnomatixInstallation.pdf", "TecnomatixReleaseNotes.pdf" & "TecnomatixHardwareRequirements.pdf" of which the release notes says that Virtual Infrastructure (VDI)  is supported
 
 The supported OS are listed in the installation guide as below:
  • Windows 10
  • Windows Vista
  • Windows 2008 R2
  • Windows 7
  • Windows 2012 R2
  • Windows 8.1




Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1709
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.0
Function: LICENSING

Ref: 002-8007476

KB Article ID# PL8007476

Contents

SummaryDetails

Associated Components

Process Simulate Installation