NX X Why is no JT output created while running run_ugtopv.bat?

2021-10-06T23:26:33Z
NX for Design

Summary


Details

Why is no JT output created while running run_ugtopv.bat?

Solution

Below are some of the checks to be taken care of:
1. JT data is only created when there is an object/objects present and involved in the part file during translation.
2. Always ensure that the solid or surface body to translate in present in the Reference set.
3. Ensure if the switch for layer setting checkLayers = true is set in the tessUG.config file. If yes then check if there is data exists in the layer filtered to be exported under below settings:

}
Filter {
layerON = "199"
}



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: TRANSLATOR
Version: V12.0.2
Function: NX_JT

Ref: 002-8007457

KB Article ID# PL8007457

Contents

SummaryDetails

Associated Components

CAD Translators