Details
User using the parts in assembly some with server name and same with IP (old method he used to follow) .
Because of which he is facing multiple issue such as wrong quantity in bill of material; where used command is not working etc..
Is there any way by which we can convert the parts properties drag from IP to server name.
Solution
The Solid Edge Data Preparation Utility is the safest method to change file properties at once.
Notes and References
9288989
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 8.164
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP14
Function: DATA_PREP
Ref: 002-8007454