User can't list vault custom properties in Windows Explorer at client machine.

2021-10-06T23:53:35Z

Summary


Details

User can't list vault custom properties in windows explorer at client but in the vault machine (share folder) can list custom properties.

Solution

- Please run the diagnostic app on client machine too and check the configuration.
- The Windows Explorer schema/ column sequence should be same on client machine and vault (server) machine.
- Use/ register the same propseed file i.e. used on vault (server) machine also on client machine for the custom properties to be displayed.

Notes and References

9306344

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEDM

Ref: 002-8007452

KB Article ID# PL8007452

Contents

SummaryDetails

Associated Components