NX X Importance of "NX_NON_MASTER" attribute.

2021-10-06T23:26:33Z
NX for Design

Summary


Details

What is the importance of "NX_NON_MASTER" attribute. Why is the Component part automatically selected by the Base View operation?

Solution

Solution:

When creating a master model drawing "NX_NON_MASTER=drawing" attribute gets created automatically and it plays an important role while placing a View. It creates an attribute called NX_NON_MASTER with value set to "drawing" to indicate it is a master model drawing.

When an assembly or a piece part is opened and a drawing is created from it  using File->New command, the master model drawing is created. To support this workflow, the master model is added as a component under drawing the part. While creating base view in Drafting, this master model is automatically selected  for view creation. User has an option to override this and manually select drawing part instead.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0
Function: DRAWING/VIEW

Ref: 002-8007437

KB Article ID# PL8007437

Contents

SummaryDetails

Associated Components

Drafting