NX X Basic Curves tracking bar pop-up is missing

2021-10-06T23:26:32Z
NX for Design

Summary


Details

While using the Basic Curves command, the tracking bar is missing.



Solution

1. With the Basic Curve dialog open, in the Menu, select 'Preferences-->User Interface'.
2. Highlight 'Layout'.
3. Select the 'Reset Window Position' icon.
The Tracking Bar pop-up should appear.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V10.0.3
Function: CURVE

Ref: 001-9329517

KB Article ID# PL8007356

Contents

SummaryDetails

Associated Components

Modeling