Details
Starting with NX 12 in some cases the output of the File => Plot command in NX causes distorted results when the used model is defined as RASTER/RTL. This also might happen when you try to use RASTER/RTL to communicate with a PCL printer.
Solution
There are several possibilities that might help to work around this behavior:
- set the additional environment variable "UGII_CGM_RASTER_ELEMENT=rle_cell" to modify the CGM output
- modify the parameters for Rendering if you are using PCL
Rendering: +PCL3GUI +RGB +QL100
Post Processing: +RGB
- check if it is possible to use another configuration for the model Setup (HPGL, PS, ...)
- copy the NXPLOT directory from NX 11 to your NX 12 installation
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: GATEWAY
Version: V12.0
Function: PLOTTING
Ref: 002-8007347