NX X Importing using a clone log to specify a name with a slash

2021-10-06T23:26:32Z
NX for Design

Summary


Details

When using 'Import Assembly into Teamcenter' or tcin_import, and using a clone log, how can the name be specified if it has a slash in it? 
For example: Clone_Name: "@DB/Screw 5/8/A"
    Where "Screw 5/8" is the ItemID.



Solution

The character following the entry, "@DB", specifies the delimiter. So a different delimiter can be used. A "#", or some other character, can be specified. 
Change:  "@DB/Screw 5/8/A"
To:  "@DB#Screw 5/8#A" 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V9.0.3
Function: CLONE_IMPORT

Ref: 001-9328349

KB Article ID# PL8007346

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX