Solid Edge Which file stores the Saved settings of the Tube properties?

2021-10-06T23:53:34Z
Design

Summary


Details

The "Tube Options" dialog provides the ability to store the "Tube properties" via the "Saved settings" functionality.  In which file will these settings be stored?

Solution

These settings will be appended to the end of the following file:

C:\Program Files\Siemens\Solid Edge 2019\Preferences\Custom.XML

Example:

before:

 </DrawingViewScales>
</SolidEdgeCustomSettings>

after:

 </DrawingViewScales>
<CustomTube><SavedTube name="abc"><Material> ... </SavedTube></CustomTube></SolidEdgeCustomSettings>

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1803
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219.0
Function: XPRESROUTE

Ref: 002-8007336

KB Article ID# PL8007336

Contents

SummaryDetails

Associated Components

Assembly Modeling