Solid Edge SEEC 're-save' with change item name does not change the item revision name

2021-10-06T23:53:33Z
DOC_MANAGEMENT

Summary


Details

During a save/upload, modifed the Item's name ( object_name ) but the Item Revision's name did not update with the same change.



Solution

The Item Revision Name is not forced to match the Item Name. 

If you want to edit the Item Revision Name you need to add it to the CPD (using attribute mapping to a custom SE property) and edit it directly. For example, with the following mapping: 

{ Dataset type="SE Part" Item_Rev_Name : ItemRevision.object_name /master=both /description="Item Revision Name"}



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEEC

Ref: 001-9326756

KB Article ID# PL8007328

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC