Solid Edge Direct model should maintain the color of part when importing through ATTI.

2021-10-06T23:53:32Z
Data Management

Summary


Details

Direct model(JT) should maintain the color of part when importing through ATTI.



Solution

Import the Solid Edge data into Teamcenter using "ATTI", it generates the JT file as well.


Before staring ATTI session set parameter "Use Solid Edge Resolution" to "0" in the translation definition file SEECtoJT.ini.

Import SE part using ATTI, the generated direct model(JT) will have same color as that of SE part.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP2
Function: SEEC

Ref: 002-8007294

KB Article ID# PL8007294

Contents

SummaryDetails

Associated Components

Teamcenter