NX Customer Defaults "Enter application where Part was Last Saved or Displayed" is gone in NX12

2021-10-06T23:26:32Z
NX for Design

Summary


Details

There was the following setting given in NX11.
The same setting isn't available in NX12 anymore.

Solution

The "Enter Application where Part was last saved or displayed" customer default was removed in NX12 to support Multiple Display Parts workflow.

"Enter Application where Part was Last Saved or Displayed" is always on by default from now on.

In NX12 upcoming license messages (e.g. because a user without a CAM license open a prt last save in Manufacturing) are not wanted and do not show up in NX1847. This was changed by PR 9212524.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V12.0
Function: PART_FILE_OPS

Ref: 002-8007282

KB Article ID# PL8007282

Contents

SummaryDetails

Associated Components

Assemblies