Solid Edge Solid Edge ST10 - Maintenance Pack 12 Announcement

2021-10-07T00:09:59Z
Data Management Manufacturing Simulation Xcelerator Share Apps Design

Summary


Details

December 10, 2018
 
Dear Solid Edge Customer: 
 
Solid Edge ST10 Maintenance Pack 12 is now available for download.
 
Sincerely,
The Solid Edge Team 
  
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge ST10 MP12
Version: 110.00.12.04
 
================
Download Location:
================
 
Solid Edge ST10 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/
 
==========
Installation:
==========
 
•        MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
•        MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
•        MSI Product Updates calculate free disk space before installing. Please be patient.
•        MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
•        MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
•        Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
•        When uninstalling, the original source media must be available to allow the recovery of previous file versions.
•        The current MSI Product Update will be the only Update listed and available for uninstallation. 
•        After the current Product Update is uninstalled the previous Product Update will become the current Update.
•        .zip files delivered with this MP such as: SESP_Server_2010_MP4.zip, SESP_Server_2013_MP4.zip, and SEECAdministratorV110.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
 
===General===
PR 9260736: Template Not Found - The specified template cannot be accessed.
 
===API===
PR 9243601: No API is available to get Normal Orientation of Arc3D present in 3D Sketch
 
===Assembly=== 
PR 9282979: Solid Edge crashes after a Quick Pick workflow
 
===Draft=== 
PR 9266456: Solid Edge crashes during the creation of a section view
PR 9301025: Text aspect ratio appears increased in printouts and translated pdf documents 
 
===Part/Sheet Metal===
PR 9232827: Solid Edge crashed when clicking to select the center point of a circle in sketch profile
 
===Translators===
PR 8551634: NX open the JT exported from SE, and the location of PMI dimension is wrong
 
===Illustrations & 3D Publisher ===
PR 9273709: Assembly part incorrectly positioned in Technical Illustrations
PR 9263316: One part not coming into Illustrations in correct orientation
PR 9295706: Parts are not coming into Illustrations in correct position
 
===Insight===
PR 9278429: Pack and Go operation not maintaining folder structure
 
===Data Management===
PR 9305230: Add Auto obsolete old revisions functionality
 
===Teamcenter Integration for Solid Edge===
PR 8394937: SEEC writes multiple SETCFunction events to the Windows Application log
PR 9270284: Crash when trying to change a custom property with dynamic LOV attached 
PR 9284480: Teamcenter Interactive does not support Dynamic LOVs
PR 9288221: Files open checked out, selected  read only all levels, Multi files select
PR 9285948: BOM is not updating correctly using this workflow
PR 9127806: Add Honor new preference to clear properties functionality
 

SFB-SOLID_EDGE-8007253
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8007253

Contents

SummaryDetails

Associated Components

Built-in Design Manager Insight Teamcenter