How to create Principal Axes in NX12

2021-10-06T23:26:32Z

Summary


Details

How to create a 'Center of Gravity' mark or the Principal Axes using the Measure tool.



Solution

1. In the Menu, select 'Analysis-->Measure'.
2. Set 'Object to Measure = Object'.
3. Select the solid body.
4. Under the Settings group, toggle 'Associative' if needed.
5. Select the right-hand edge of the pop-up Information table to expand it. 
This will expose the Geometry and Requirements columns.
6. In the 'Center of Gravity' and/or the 'Principal Axes' row, toggle the icon in the Geometry column to create the geometry on 'OK' or 'Apply'.
7. OK or Apply the Measure dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: INFO_ANALYSIS

Ref: 001-9321517

KB Article ID# PL8007243

Contents

SummaryDetails

Associated Components