NX X NX Pattern Feature of Holes "Simple" Method

2021-10-06T23:26:32Z
NX for Design

Summary


Details

A Pattern Feature of Holes is created using a "Simple" pattern method.

The pattern does not take into account the depth limit defined in the hole



Solution

A Pattern Feature of Holes is created using a "Simple" pattern method.
The documentation of this method states that associative trim limits such as:

•Until Selected-
•Until Next-
•Until Extended-

and so on will not be applied.

The "Simple" method is designed for faster performance with a large number of instances on the same target body. Local operations such as trimming of the Hole's tool body in this case, cannot be applied in "Simple" Pattern method.
Use the "Variational" method to produce the desired result.





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: FEATURE_MODEL

Ref: 002-8007230

KB Article ID# PL8007230

Contents

SummaryDetails

Associated Components

Modeling