Solid Edge Error uploading templates

2021-10-06T23:53:29Z
Data Management

Summary


Details

The following error occurs when attempting to add Solid Edge templates to Teamcenter: 
Import Solid Edge Templates 
An unexpected error occurred while importing the Solid Edge templates. Correct the issue using the information captured in the log file and then import your templates.



Solution

This error will occur if the client workstation being used to upload the templates does not have the correct file associations for the Solid Edge file types. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEEC

Ref: 001-9317174

KB Article ID# PL8007208

Contents

SummaryDetails

Associated Components

Teamcenter