NX Sheet Metal - Normal Cutout:
We are limited to having one target body. This means we can only cut through one sheet metal plate.
Solution
To cut through multiple sheets:
1. Create Normal Cutout selecting one sheet body
2. Make Sketch external
3. Copy/Paste Normal Cutout feature
4. On 'Paste Feature' form - References - Original Parent - select 'Target Body'- select new target plate,
This keeps the original sketch associative to the two Normal Cutout features
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: XP64_SP2
Product: NX
Application: NX_SHEET_METAL
Version: V12.0.2
Function: NORMAL_CUTOUT
Ref: 001-9309485