How to ensure that mesh colours defined in the context of a '.fem' file are also seen in the context of any associated '.afm' or '.sim' file?
Solution
In the context of the '.afm' or the '.sim' file (as required), set the following option:
Menu
Preferences
Model Display
Element (tab)
Display, Color Basis = FEM Mesh Color
With this option defined, the colour of a mesh in the context of a '.afm' file or '.sim' file will be consistent with the colour of that same mesh in the context of the associated '.fem' file.
Notes