NX X Vector and/or point is either suppressed or modeled away warning

2021-10-06T23:26:31Z
NX for Design

Summary


Details

How to resolve the following warning on sketch feature? 

"Parent of the point is either suppressed or modeled away / vector is either suppressed or modeled away."



Solution

(1) Edit the sketch.

(2) Once in Edit mode, bring up the Reattach Sketch command.

(3) In the Reattach Sketch dialog:
           To fix the point issue:
                     Use Sketch Origin option to re-specify another point.
           To fix the vector issue:
                     Use Sketch Orientation option to re-specify another vector.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V12.0
Function: SKETCHER

Ref: 001-9313175

KB Article ID# PL8007107

Contents

SummaryDetails

Associated Components

Modeling