NX Setting up a Post to Output TCP, RTCP and 3+2 Machining Mode.

2021-10-06T23:26:31Z
NX for Manufacturing

Summary


Details

What can be done to specify whether G68 , G68.2 , G43.4 or G43.5 is included in the posted output? How is the post configured to set the CSYS as fixed on table or on machine?

Solution

Create a new multi-axis Post Builder post selecting the Fanuc 30i Advanced Controller . Edit the PB_CMD_customize_output_mode Custom Command in the Start of Program event as noted in the proc. It is important to create the post using the newest version of Post Builder that can be had in order to get the most developed TCL code.


Notes

KB Article ID# PL8006989

Contents

SummaryDetails

Associated Components

Post Builder