Is it possible to display a link between the Family Of Parts Master and the Populated Members in Teamcenter RAC?
Solution
No, it's not possible to display a link between the Family Of Parts Master and the Populated Members in Teamcenter RAC. Yes, it is possible to display a reverse link between the Populated Members and it's FOP Master in Teamcenter RAC.
The relation we use in Teamcenter is:
Real Name SE Interpart Family Links
Display Name Solid Edge Part Family Members
Comments FOP
Set this Relation on the Item Revision via the TC Options dialog and the SE Part_DefaultChildProperties preference. Add the Relation to the Show Relations of the Item Revison General tab and to the preference.
Now we can see in the Item Revision the relation. For eaxmple ItemRev 000229/A is the Master FOP, 000230/A is member 1 and 000231/A is member 2. Note that each member's Item Revision has the pseudo line item (the reverse link) back to the master file.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 10_1709
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP15
Function: SEEC
Ref: 001-9302168