Dear Siemens PLM Software Customer,
We are pleased to inform you that RobotExpert controllers for "ABB, FANUC, KUKA, CLOOS, COMAU, DEFAULT, DENSO, EPSON, IGM, KAWASAKI, MITSUBISHI, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, TOOLS/UPLOAD_ROBCAD_ROBOTIC_PROGRAM, UNIVERSAL, USER_INVERSES/7R_AXIS_INVERSE, YASKAWA" are available for download from https://download.industrysoftware.automation.siemens.com.
See RobotExpert_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'Change_Logs' folder directly under the 'Robot_Controllers' folder.
Use the following steps to download.
Note: A valid WebKey account is required.
(URL: https://plmapps.industrysoftware.automation.siemens.com/webkey/)
In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/
WebKey Username: [your WebKey user ID]
WebKey Password: [your WebKey password]
Select the Download tab
In the Product Filter area scroll down to Tecnomatix Products
Select Tecnomatix Products
Expand Product updates
Expand RobotExpert/
Expand Robot_Controllers/
Expand V13.0/, V13.1/, V13.1.1/, V13.1.2/, V14.0/, V14.0.1/, V14.0.2/, V14.1/, V14.1.1/ or V14.1.2/
Expand ABB, FANUC, KUKA, CLOOS, COMAU, DEFAULT, DENSO, EPSON, IGM, KAWASAKI, MITSUBISHI, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, TOOLS/UPLOAD_ROBCAD_ROBOTIC_PROGRAM, UNIVERSAL, USER_INVERSES/7R_AXIS_INVERSE or YASKAWA
Download the file(s):
RobotExpert_13.0_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_13.0_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_13.0_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_13.1_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_13.1_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_13.1_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_13.1.1_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_13.1.1_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_13.1.1_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_13.1.2_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_13.1.2_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_13.1.2_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.0_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.0_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.0_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.0.1_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.0.1_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.0.1_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.0.2_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.0.2_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.0.2_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.1_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.1_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.1_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.1.1_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.1.1_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.1.1_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.1.2_7R_AXIS_INVERSE_64BIT_v1.1.8_03_10_2018.exe
RobotExpert_14.1.2_ABB_RAPID_64BIT_v3.16.1_09_11_2018.exe
RobotExpert_14.1.2_CLOOS_CAROLA_64BIT_v1.21_11_04_2018.exe
RobotExpert_14.1.2_COMAU_PDL_64BIT_v4.2.2_01_06_2018.exe
RobotExpert_14.1.2_DEFAULT_64BIT_v2.37_31_10_2018.exe
RobotExpert_14.1.2_DENSO_PACSCRIPT_64BIT_v2.1_19_10_2018.exe
RobotExpert_14.1.2_EPSON_SPEL_64BIT_v1.18_11_04_2018.exe
RobotExpert_14.1.2_FANUC_RJ_64BIT_v2.50.1_31_10_2018.exe
RobotExpert_14.1.2_FANUC_RJ_64BIT_v2.50.2_09_11_2018.exe
RobotExpert_14.1.2_IGM_INS_64BIT_v1.25_11_04_2018.exe
RobotExpert_14.1.2_KAWASAKI_AS_64BIT_v2.59_10_09_2018.exe
RobotExpert_14.1.2_KUKA_KRC_64BIT_v3.63.1_09_11_2018.exe
RobotExpert_14.1.2_MITSUBISHI_MELFA_64BIT_v0.1_20_04_2018.exe
RobotExpert_14.1.2_NACHI_SLIM_64BIT_v4.0_31_10_2018.exe
RobotExpert_14.1.2_NC_CODE_64BIT_v1.25.3_11_04_2018.exe
RobotExpert_14.1.2_OLP_TOOL_64BIT_v15.1_28_09_2018.exe
RobotExpert_14.1.2_PANASONIC_CSR_64BIT_v1.12_11_04_2018.exe
RobotExpert_14.1.2_STAUBLI_VAL_64BIT_v1.22_31_10_2018.exe
RobotExpert_14.1.2_UNIVERSAL_URSCRIPT_64BIT_v2.15_27_06_2018.exe
RobotExpert_14.1.2_UPLOAD_ROBCAD_ROBOTIC_PROGRAM_64BIT_v2.6_04_07_2018.exe
RobotExpert_14.1.2_YASKAWA_INFORM_64BIT_v4.10_31_10_2018.exe
To Install:
Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the RobotExpert installation).
Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens PLM Software
SFB-TECNOMATIX-8006934
PR N/A
Product Information: