How to make a Reuse Feature Template into a Reusable Part

2021-10-06T23:26:31Z

Summary


Details

How to make a Reuse Feature Object Template into a Reusable Part. 
A part listed in the Reuse Library folder is missing the 'Create KRX' option. It is listed as a Feature Object Template. Feature Object Templates do not have the ability to create a KRX file. How can I make a Feature Object Template into a Reusble Part so I can create a KRX file?



Solution

1. In Teamcenter, make sure the part exists in the Reuse Library folder.
2. In NX, Perform a 'File-->Open' to open the Reusable Feature Object Template.
3. Select 'File-->Properties'.
4. Delete the attribute: REUSE_LIBRARY_OBJECT_TYPE
5. OK and close the Properties dialog.
6. Save and Close the part.
7. In the Reuse Library tab, 'MouseButton3-->Refresh'.
Now the part should be listed in the Reuse Library folder and have the option, 'MB3-->Create KRX'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V11.0.2
Function: REUSE_LIBRARY

Ref: 001-9302130

KB Article ID# PL8006925

Contents

SummaryDetails

Associated Components