Solid Edge Change "Author" name for new Solid Edge drawings

2021-10-06T23:53:17Z
DRAFT

Summary


Details

The Author for new Drawings is not correct after transfering a machine from one person (User 1) to another (User 2) and even the Solid Edge Templates are updated to the new Author - User 2,  the former Author (User 1) being overwritten.



Solution

The Author property is a Solid Edge System Property that is tied to the Windows Profile User ID.  Therefore this value cannot be changed unless the Windows Profile User ID value is changed. 

Disabling or deleting the "User 1" User Profile will resolve the problem.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP11
Function: OTHER

Ref: 001-9285922

KB Article ID# PL8006892

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS