Simcenter 3D Solutions Simcenter 3D Motion Animation with Flexible Body

2021-10-06T23:26:31Z
Simcenter 3D

Summary


Details

In Simcenter 3D Motion, when there are one or more flexible bodies, the animation can take minutes to start after pressing the Play button.

Solution

By default, the animation uses the absolute max/min values. This can be changed in the Motion Preferences. To access Motion Preferences, go to Menu-->Preferences-->Motion


In the Motion Preferences dialog, uncheck the option to Use Absolute Min/Max Values for Flexible Body


Click OK in the Motion Preferences dialog and animate the solution. 

Notes

KB Article ID# PL8006869

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow