Solid Edge ST10 - Maintenance Pack 11 Announcement

2021-10-07T00:09:59Z

Summary


Details

October 29, 2018
 
Dear Solid Edge Customer: 
 
Solid Edge ST10 Maintenance Pack 11 is now available for download.
 
Sincerely,
The Solid Edge Team 
  
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge ST10 MP11
Version: 110.00.11.04
 
================
Download Location:
================
 
Solid Edge ST10 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/
 
==========
Installation:
==========
 
•        MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
•        MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
•        MSI Product Updates calculate free disk space before installing. Please be patient.
•        MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
•        MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
•        Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
•        When uninstalling, the original source media must be available to allow the recovery of previous file versions.
•        The current MSI Product Update will be the only Update listed and available for uninstallation. 
•        After the current Product Update is uninstalled the previous Product Update will become the current Update.
•        .zip files delivered with this MP such as: SESP_Server_2010_MP4.zip, SESP_Server_2013_MP4.zip, and SEECAdministratorV110.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
 
===Assembly=== 
PR 9149569: Crash by using function "Occurrence-> GetIncludeInBom"
PR 8390834: "Capture Fit" in ST10 does not automatically align to planes
PR 9260675: Assembly Relationship display is wrong with Decimal symbol regional set Comma
PR 9152181: Performance problems between ST7 and ST9 with Ribbon Bar
PR 9249837: More fixes to help reduce the chances of accidental component placement from Pathfinder
 
===Draft=== 
PR 9227323: Problem with expanded Character spacing, when printing or saving as PDF
 
===Part/Sheet Metal===
PR 9157575: Sheet Metal Part Will Not Flatten
PR 9254343: Opening the provided file will crash immediately after showing the part
 
===Translators===
PR 8387280: Error during Solid Works data migration - "migration terminated" 
PR 9194495: After updating SE ST10 with MP8 User can't do migration of SolidWorks draft 
PR 9210245: Block Labels not exported to DXF with correct color
PR 9018880: Cannot make Sync edit on Sheet Metal if another part was edited and closed
PR 8859606: Certain parts won't display in imported IFC
 
===Illustrations & 3D Publisher ===
PR 9263316: One part not coming into Illustrations in correct orientation.
 
===Data Management===
PR 8382986: Slow performance with Solid Edge DM Search
PR 9145113: Unable to set Custom Properties when ProSeed file is on network drive
 
===Teamcenter Integration for Solid Edge===
PR 9191395: Mapped properties / master=cad will modify Solid Edge property when cleared in RAC
PR 9257251: 3D dataset is not inherited when revised/copied in Structure Editor 
PR 9261228: Revision field grayed out during Save to Existing
PR 9127806: Honor new preference to clear properties
 

SFB-SOLID_EDGE-8006800
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8006800

Contents

SummaryDetails

Associated Components